Cancel
Showing results for 
Search instead for 
Did you mean: 

SOL 601

Pioneer
Pioneer

I am not being able to view the results, even though the op2 file has generated.

Kindly suggest a way to rectify the problem.

6 REPLIES 6

Re: SOL 601

Phenom
Phenom

.op2 file is generated even if analysis has crashed. Check your analysis has actually succesfully completed

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: SOL 601

Pioneer
Pioneer
I have checked for errors/fatal in the f06 file, and it doesn't show up
any, except for some warning.

Re: SOL 601

Legend
Legend

SOL 601,129

Solution > Case Control > Output Requests > Sorting > For each request, change sorting type "default" to SORT1

Re: SOL 601

Pioneer
Pioneer

Thanks. I have updated the SORT1 option to all output request. Some warnings exist still.

Re: SOL 601

Legend
Legend

Are you still unable to see the results? or those warning a different issue? 

Try clearing the T(*) values from MATT1 as the warning suggest and see if this helps in any ways.

Feel free to share the *.dat file if you want someone to look into this for you.

Highlighted

Re: SOL 601

Genius
Genius

- Do you check if it is statically determinated? Check if there are rigid modes using a SOL103.

- A static linear solution give resonable results?

- What happen if you apply only 10% of the load on your non-linear simulation? Does the simulation run properly and give you correct results?