Cancel
Showing results for 
Search instead for 
Did you mean: 

Solver input file not found

Innovator
Innovator

Hi,

When I click on "Solve" there is no error  of meshing or boundary conditions but in the solution monitor,this error occurs.

Can you help me please?

 Error.PNG

Regards,

Sonny

3 REPLIES 3

Re: Solver input file not found

Phenom
Phenom

the nastran input file does not exist in the specifiedf folder is my guess !

Have you actually check what you have in specifiedf folder ?

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Solver input file not found

Innovator
Innovator

@selex_ct,Thank you for your reply,Yes of course.

Re: Solver input file not found

Siemens Creator Siemens Creator
Siemens Creator

In the ribbon bar under "Home", hit the SOLVE button  and select "Write solver input file". In the text window that appears, scroll up to find the directory the file was written to. It should say something like "Writing file <path_to_file>". Confirm that the <path_to_file> is the same as .\Solution_1 or whatever you want it to point it.