Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Surface contact with springs using universal connector

How to setup a problem with universal connector option for spring contact. I have a component that has contact with a spring. when i apply normal force, the spring stiffness has to resist from other side like a suspension system. how can i apply spring into the model during static stress analysis in nx nastran?

1 REPLY 1

Re: Surface contact with springs using universal connector

Gears Phenom Gears Phenom
Gears Phenom

CBUSH element plus RBE2 or RBE3 spider.