Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Time dependent force

Pioneer
Pioneer

Hello,

 

How do I add a time varying force? I checked the documentation but all it says is TLOAD1 or 2, how do I add these to my simulation?

3 REPLIES 3

Re: Time dependent force

Siemens Phenom Siemens Phenom
Siemens Phenom

You need a DLOAD case control to select the dynamic load. The SID specified in case control can directly reference the TLOADi bulk data entry.

 

The TLOADi entry then specifies the type of excitation (Load or enforced displacement/velocity/acceleration), gives reference to a TABLEDi field that specifies time vs. scale factor, and an EXCITEID. Any load entries (i.e. FORCE, PLOAD, etc.) that have an SID matching the EXCITEID on a TLOADi will have their magnitudes scaled with time accoring to the TABLEDi data.

Re: Time dependent force

Pioneer
Pioneer

Thanks for the reply, but how do I do all that? Right-click on the Solution, then Edit..., then Case Control or Bulk data?. I don't know how to do that. Can you explain it to me in little steps, please?

Re: Time dependent force

Siemens Phenom Siemens Phenom
Siemens Phenom

Sorry. You posted the question in the NX Nastran forum, so I answered in terms of Nastran. If you want to know how to set this up in NX, the post should really be in the NX CAE forum.

 

What version of NX are you running, and what type of solution are you setting up?