Cancel
Showing results for 
Search instead for 
Did you mean: 

Topology Optimization SOL 200 - What do the optimization graphs show?

Gears Valued Contributor Gears Valued Contributor
Gears Valued Contributor

Dear experts,

 

please tell me in detail what the optimization graphs show? (see attached picture)

 

FYI:

  • Design Objective: Compliance (CMPLNC) / MIN
  • Design Constraint: Design Area Weight (DWEIGHT) / Lower Limit: 300 g; Upper Limit: 330 g
  • Manufacturing Constraint: 2 Planar Symmetry (SYMP) and Minimum Member Size (MINS) 6 mm

Which graph shows what?

What do the numbers on the vertical axis mean?

And what exactly does it mean when the graph proceeds horizontally over the design iterations?

 

Kind regards

 

1 REPLY 1

Re: Topology Optimization SOL 200 - What do the optimization graphs show?

Siemens Genius Siemens Genius
Siemens Genius

The Objective Plot shows the value of the Objective Function (in your case this is the Compliance value for the structure) as a function of number of Optimization Design Cycles (or iterations) that were evaluated.  The Maximum Critical Constraint Plot shows a Normalized value from 0 to 1 for the constraint that was most critical at each optimization design cycle. In your case, you only have one Design Constraint (DWEIGHT), so this plot shows the normalized design area weight (DWEIGHT) over each cycle. If you had more Design Constraints, the solution could have a different Critical design constraint from cycle to cycle. To show somrthing to the user, the graph only show the Most Critical one (whatever it is) at each cycle.