Cancel
Showing results for 
Search instead for 
Did you mean: 

Topology optimization with parameter Inertia Relief

Creator
Creator

Hi,

I would like to ask you if is possible to use parameter 'Inertia Relief' (SOL101) in combination with Topology optimization (TOSCA-based topology optimization)?

 

Thank you!

Frank

 

PS. Alternatively; will be the parameter 'Inertia Relief' supported in the new NX Nastran-based topology optimization?

3 REPLIES 3

Re: Topology optimization with parameter Inertia Relief

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hi,

Our implementation of the TOSCA Top Opt does not support Inertia Relief as it was not the full TOSCA functionality.

The NXN 11 Top Opt also does not support this. Due to the large changes for NXN 12and the amount of work this entails, this piece of functionality has had to be dropped of the list and onto the NXN 13 plan.

 

Hope that helps,

Guy Wills

Topology Optimization Product Manager

Guy Wills

Re: Topology optimization with parameter Inertia Relief

Creator
Creator

Hi,

thanks for the information!

 

Frank

Re: Topology optimization with parameter Inertia Relief

Pioneer
Pioneer

HI
Does NX13 remove topology optimization?