Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

*** USER FATAL MESSAGE 311 (IFPDRV) NON-UNIQUE FIELD 2 ON BULK DATA ENTRY CTETRA 77302175

Experimenter
Experimenter

i am having these error ,can any one suggest me to resolve this error....

 

3 REPLIES 3

Re: *** USER FATAL MESSAGE 311 (IFPDRV) NON-UNIQUE FIELD 2 ON BULK DATA ENTRY CTETRA 77302

Gears Phenom Gears Phenom
Gears Phenom

Read error messages before posting question on forum. The answer is given in this error message, check element with this number in .dat file, maybe you have two elements with the same ID.

You can post .dat file here.

Re: *** USER FATAL MESSAGE 311 (IFPDRV) NON-UNIQUE FIELD 2 ON BULK DATA ENTRY CTETRA 77302

Siemens Phenom Siemens Phenom
Siemens Phenom

On an element definition card (i.e. CTETRA), Field 2 is the element ID number (EID):

 

https://docs.plm.automation.siemens.com/tdoc/scnastran/2019_1/help#uid:index_QRG:id511476:id507806

 

"Non-unique field 2" means that there are two (or more) elements in the input deck that have the same ID number.

Re: *** USER FATAL MESSAGE 311 (IFPDRV) NON-UNIQUE FIELD 2 ON BULK DATA ENTRY CTETRA 77302

Experimenter
Experimenter

thank u