dentability analysis using NX nastran

Experimenter
Experimenter

Hi all,

is there any of u had perform dentability analysis using NX nastran -let says a hemisphere identer hit a plate. deformation and oil canning will be then observed?

 

one more thing...i also try to create hemisphere to illustrate identer but only get a circle.

1 REPLY 1

Re: dentability analysis using NX nastran

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

 

What do you call dentability? Do you use NX for modeling?, If so, for an hemisphere, you only need to go to the modeling then menu->insert->design feature-> sphere.

 

Then use a plane to divide the sphere in two.

 

Let me get more information about dentability so I can help?

 

Naguib