Cancel
Showing results for 
Search instead for 
Did you mean: 

what is the difference between RBE2 and RBE3 elements?

Pioneer
Pioneer

Hi

Could someone tell me where should i use RBE2 element and RBE3 Element.Where should i use them.

Please help me understand both of them with an simple example.

2 REPLIES
Highlighted

Re: what is the difference between RBE2 and RBE3 elements?

Siemens Phenom Siemens Phenom
Siemens Phenom

The following comments assume default element dof settings.

 

In a RBE2, grid 1 is the independent and grids 2-n are dependent. The relative position of grids connected by the element does not change during the analysis.

 

In a RBE3, grid 1 is the dependent and grids 2-n are independent. Grids 2-n are free to mode relative to each other. The displacement of grid 1 is the weighted average of the displacements of grids 2-n.

 

RBE2 is used to represent a rigid connection. RBE3 is used for load distribution or a flexible connection.

 

See R-Type Elements in the Element Library Reference in the online help.

 

Re: what is the difference between RBE2 and RBE3 elements?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

To learn more about RBE2 vs. RBE3 elements take a look to my blog in the following address:

https://iberisa.wordpress.com/2015/10/13/rbe2-vs-rbe3-on-femap-with-nx-nastran/

Best regards,
Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/