Cancel
Showing results for 
Search instead for 
Did you mean: 

write expression

Experimenter
Experimenter

Hi

 

i need to apply a pressure according the axis node position.

i don't find how write the expression?

 

Thank for your help

 

Frçs

1 REPLY

Re: write expression

Genius
Genius

First of all define  a coordinate system using "Model, Coord Sym...". Then create the load accoding the type you need and choose pressure put 1 as the load pressure value and select the coordinate system you want to use and the variable method... Advanced...Equation...and write the equation using the symbol for the indipendent variable e.g. !X (or !Y or !Z). See also point

4.4.7  Numerical Input - The FEMAP Calculator of the help

 

Best Regards

AMinati