Cancel
Showing results for 
Search instead for 
Did you mean: 

Do I need to creat battery cell before creating each battery module ?

Pioneer
Pioneer

Dear @

        I have created a battery cell from .tbm file , and set  Battery Module Module Configuration successfully  for the first Module Module .

       However , There is no battery cell to  set the  property of Battery Module Module Configuration for the second Module Module .

       So, do I need to creat the battery cell for each Battery Module  ?QQ图片20190103175610.png

 

 

 

 

1 REPLY 1

Re: Do I need to creat battery cell before creating each battery module ?

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi Jianlin:

 

You do not need to create another Battery cell . In the new Battery Module go to Battery Module 2 or Copy of Battery Module select > Module Configuration > Battery Cell > Select the Battery Cell as shown in the picture.

Hope that is helpful.

Untitled.png

Thank you.

 

Kind Regards,

Kaushik