Cancel
Showing results for 
Search instead for 
Did you mean: 

Microsoft's Surface Hub Features Catchbook

Community Manager Community Manager
Community Manager

Microsoft and their new Surface Hub decided to showcase Catchbook on its very large display. Catchbook is looking wonderful and bold running on Surface's near 4K resolution (3840 x 2160.) I for one would love to test out Catchbook on this huge display which stretches 46.12” x 86.7” x 4.15” or (1,171.5mm x 2,202.9mm x 105.4mm)

 

 

See it for yourself here: