Cancel
Showing results for 
Search instead for 
Did you mean: 

Catchbook Known Issues

Siemens Legend Siemens Legend
Siemens Legend

Nobody's perfect! These are some of the issues we have found with the current versions of Catchbook. 

 

  • There can be a delay between when you subscribe and when you see the licensed functionality available in the app.  If this happens to you, wait 5 minutes then restart the app - everything should work after that.

 

You can check this list to see if we are already tracking an issue you find:

 

D-01334

Windows: Virtual keyboard does not display when editing dimension (have to highlight text first) Fixed

D-01615

Windows: Double tapping a Catchbook file in the OS will not open unless Catchbook is already running - Fixed in 1.5

D-02037

Can't drag items with mouse in Navigator - Fixed

B-03597

Android: press drag is not working well in navigator on some Android devices

D-02333

More buttons appears when dimension selected - Fixed

D-02273

Dragging the last Catchbook before the active Catchbook sometimes causes a crash - Fixed

D-02415

Highlighter pen direction wobbles back and forth, makes a rounded corner when changing direction

B-03578

Catchbook beta only runs on devices with an ARM processor (Runs on some Intel devices with emulation)

D-02480

The Catchbook binder order changes when maximizing the Window size (Windows only)

D-02623

Shake and Break does not work when there is a lot of content on the page

D-02698

Page content shrinks into top left - Fixed

D-02721

Windows free trial not working in some cases - Fixed

D-02617

Crash on first launch on Windows 8.1

D-02722

Close icon not working sometimes on WinRT Help dialog, have to restart app

D-02724

Tutorial Button text not displayed correctly on start-up - Fixed

D-02541

Small images appear large when added to page - Fixed

B-06852

Binder Thumbnail quality is low

D-02233

Angle Dimension Extension lines not extending correctly

D-03846

Context menu overlaps dimension edit box in some cases

D-04146

Catchbook will not run on some Android 7.0 devices - Fixed in 1.5

D-02722

Sometimes the close icon does not work in the info dialog

D-05362

iOS button pushes are slow to react

D-04059

Stylus tap does not deselect trace image when drawing mode is off

D-05402

Circles centers are not aligning when they are created

D-02139

Difficult to reposition small parallel dimension

D-02236

New page is always added to the end of the binder

 

 

14 REPLIES

Re: Catchbook Known Issues

Experimenter
Experimenter

iOS app not remembering purchase of Saver Pack. Purchased yesterday but upon leaving app and returning, the store items appear as available to buy again, the advanced tools are not available for use. The 'Restore' button does not restore the purchase. Tested on iPhone 6 and iPad Air.

Re: Catchbook Known Issues

Experimenter
Experimenter
It happens the same on iPad Pro.
I would like to point as well that the palm rejection with Apple Pencil fails repeatedly. The view jumps as soon as you rest the palm. This is the only app that I've had problems with palm rejection until now.
Another thing that I find inconvenient is that the freeform stroke is very irregular using the Pencil. The slower you draw the worst it gets. It's very difficult to write text with it.
I think that this app can be great for designers, but right now these fails make it very hard to use.

Re: Catchbook Known Issues

Siemens Legend Siemens Legend
Siemens Legend

@rimeiQuer, @Andy_Pollard.  Thank-you for letting us know about these issues.

 

It looks a few people are seeing glitches with iOS purchasing.  We have all hands on deck trying to resolve the problem.

 

It would be a great help if you could let us know some details:

  • Which country do you access the App Store from?
  • Which functionality did you subscribe to (Saver Pack, Drawing or Publishing)?
  • Were you part of our iOS beta program?
  • Did you install on more than one device?
  • What device did you install on?

 

We have seen one workaround, however it doesn't work for everyone:

Try hitting the Purchase button again and then cancelling the password/touch identification screen.  In some cases this restores the functionality.  If it works, you have to do this every time you re-start the app.

 

We'll keep you posted as we get to the bottom of this issue...

 

Re: Catchbook Known Issues

Experimenter
Experimenter
Hello TJ, thank you for your fast response.

- Which country do you access the App Store from? Spain
- Which functionality did you subscribe to (Saver Pack, Drawing or Publishing)? Saver Pack
- Were you part of our iOS beta program? No
- Did you install on more than one device? Yes
- What device did you install on? iPhone 6, iPad Pro. 12.9 inch

The workaround doesn't work for me. I even purchased it twice hoping that being a subscription it would only be charged once. I think that the problem started when I purchased the app for the iPhone 6 after the iPad Pro.

Re: Catchbook Known Issues

Experimenter
Experimenter
  • Which country do you access the App Store from? UK
  • Which functionality did you subscribe to (Saver Pack, Drawing or Publishing)? Saver Pack
  • Were you part of our iOS beta program? No
  • Did you install on more than one device? Yes
  • What device did you install on? iPhone 5, iPhone 6, iPad Air 

Re: Catchbook Known Issues

Siemens Legend Siemens Legend
Siemens Legend

@Andy_Pollard and @rimeiQuer thanks for the info.  If anyone else out there is seeing the issue, we'd love to hear from you as well... 

Re: Catchbook Known Issues

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I’m using Sony Z3 Tablet Compact and Sony Z5 Dual Premium with latest Android 6, why from the Play Store showing not available for my devices?

Re: Catchbook Known Issues

Siemens Legend Siemens Legend
Siemens Legend

Hi @DTSChan!

 

It may be due to where you live. Currently Catchbook is only available in the following countries:

 

Australia, Belgium, Canada, France, Germany, Hungary, Italy, Japan, Luxemburg, Netherlands, Poland, Romania, Russia, Spain, Sweden, Switzerland, United Kingdom, United States

 

Hope that answers your question.

Re: Catchbook Known Issues

Siemens Legend Siemens Legend
Siemens Legend

Hi @rimeiQuer,

 

We have an update in the iOS store.  It would be great if you could update Catchbook and then report back.  It is still not clear whether this fix is working in all cases.  If there is anyone else out there seeing problems, we'd love to hear from you too.

 

After the update:

  • What happens when you open a page and hit the triangular recognition button on the left – does the store page still appear?
  • What version is installed?
    • Open a  page, hit “…”, then “i”, then tap the about tab to see the version
  • Did you cancel the subscription?
    • Even if you did, it should still work as you are within the trial period

 

Some people may experience the problem even after the update.  We’ll only know if it is fixed for sure by trying it again tomorrow. 

Download Catchbook:

Download Catchbook on iOS Download Catchbook on Android Download Catchbook on Windows 10 Image Map