Showing results for 
Search instead for 
Did you mean: 

Background image support


It would be nice from a "scale" point of view to be able to turn on grid background or allow an image to fill the sheet background. That way you can get a sense of scale and also have some "ruler" lines for those of us that like to write across a straight line instead of the free inking with the text being scribbled across the screen.




Siemens Legend

Thanks fot the suggestion.  Do you think it would help if the curves snapped to the grid points?


I think having an option to snap to grid would be beneficial. Making it snap if the grid was on I feel would annoy people. Having the ability to size the grid is important and maybe even define an area of the sheet/page that grid resides in would be productive as well. That way you can have a text/note area and then drawing area.

Siemens Dreamer

I would lik extend the visable scale which is a great idea. I would like to see a scale option 1:5, 1:10, 1:20, 1:50, 1:100. Please let me know if I am missing this option already.

Siemens Legend

 @Mr_Hayes, we don't have that option yet. But thanks for the feedback.

Siemens Legend

We have added a grid in Catchbook 1.5. See the post here.

Top Kudoed Authors