Cancel
Showing results for 
Search instead for 
Did you mean: 

TEXT / ANNOTATION Function

Valued Contributor
Valued Contributor

Dear Catchbook users,

 

maybe it would be helpfully to add a TEXT / ANNOTATION function? Such a function should activate the default mobile device keypad and should add the input as real text string onto  the sketch. Similar to the line function it should be equipped with a selector function for font and colors. Such an added text should be exported as text string entity in the SVG or DXF export.

 

Regards

 

Matthias

Comments
Siemens Legend

Thanks for the feedback. Typed text is something that we are working on.

Dreamer

Well, I'd assume it is more sensible to use hand writing recognition. (like the one from MyScript and keyboard input as an alternative).But I a agree, anotations and labelling lines, as well as arrows would be great.