Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap 101 for Femap v11 Classroom Exercises - Lesson 13 through Lesson 21 - Rev A

Siemens Phenom Siemens Phenom
Siemens Phenom

The attached Femap 101 hands-on workshops accompany the following Femap 101 for Femap v11 lessons:

 

Lesson 13 - Loads

Lesson 14 - Model Display and Visualization

Lesson 15 - Analysis Set Manager

Lesson 17 - Contour Display

Lesson 18 - Free Body Diagrams

Lesson 19 - XY Plotting Using the Charting Pane

Lesson 20 - Midsurfacing

Lesson 21 - Assembly Modeling

Lesson 24 - Laminate Shell Composite Modeling

 

Please note that there are no specific workshops for Lesson 12 - Constraints and Lesson 16 - Post-processing Overview, as these subjects are covered throughout the majority of the Femap 101 exercises.

 

You will also need to download the class exercises for Exercises 1-7 so that you have the complete file structure needed for the Femap 101 class.

 

The Student Workbook folder has the hands-on exercise instructions as PDF files.  These files are formatted such that the open PDF file can be arranged to the side of the Femap session as shown below, removing the need to have a printed version.

 

8-26-2013 7-51-19 AM.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development
1 REPLY

Re: Femap 101 for Femap v11 Classroom Exercises - Lesson 13 through Lesson 21 - Rev A

Experimenter
Experimenter

Thank you