Cancel
Showing results for 
Search instead for 
Did you mean: 

Femap 101 for Femap v11 Classroom Exercises - Lesson 7 through Lesson 11 - Rev A

Siemens Phenom Siemens Phenom
Siemens Phenom

The attached Femap 101 hands-on workshops accompany the following Femap 101 for Femap v11 lessons:

 

Lesson 7 - Meshing Overview

Lesson 8 - Line Element Meshing

Lesson 9 - Surface Meshing

Lesson 10 - Solids Meshing

Lesson 11 - The Meshing Toolbox

 

Please note that there is no workshop for Lesson 6 - Properties, as this subject matter is covered throughout the majority of the Femap 101 exercises.  Lessons 1 through 5 should also be downloaded and installed as this contains the entire file structure for the class.

 

The Student Workbook folder has the hands-on exercise instructions as PDF files.  These files are formatted such that the open PDF file can be arranged to the side of the Femap session as shown below, removing the need to have a printed version.

 

8-26-2013 7-51-19 AM.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development