Showing results for 
Search instead for 
Did you mean: 

Femap 101 for Femap v11 Classroom Exercises - Lesson1 through Lesson 5 - Rev A

Siemens Phenom Siemens Phenom
Siemens Phenom

The attached Femap 101 hands-on workshops accompany the following Femap 101 for Femap v11 lessons:


Lesson 1 - The FEA Modeling Process Using Femap

Lesson 2 - Overview of the Femap User Interface

Lesson 3 - 2D Geometry Creation and Editing

Lesson 4 - 3D Geometry Creation and Editing

Lesson 5 - Materials


The Student Workbook folder has the hands-on exercise instructions as PDF files.  These files are formatted such that the open PDF file can be arranged to the side of the Femap session as shown below, removing the need to have a printed version.


8-26-2013 7-51-19 AM.jpg

Best Regards,
Chip Fricke
Principal Applications Engineer - Femap Product Development