Cancel
Showing results for 
Search instead for 
Did you mean: 

Allow Copy-Pasting Images in messages

Phenom
Phenom

Clicking the Photos button and browsing to images then waiting the image to load and finally clicking Done is a painful and time consuming process.

 

Please allow simple copy-pasting from clipboard into the message.

 

This would be a great relief and will also encourage users to use more images in their replies making the posts more useful and clearer.

 

The pasted image can then be automatically be stored to the user's profile as is done currently.

 

Thanks.

3 REPLIES

Re: Allow Copy-Pasting Images in messages

Experimenter
Experimenter

Yes, this should be done in a way that images with a certain filesize and dimensions would be restricted. Rest are allowed.

Re: Allow Copy-Pasting Images in messages

Community Admin Community Admin
Community Admin
@fsarim @Tushar I agree with you that that would be much easier for users and increase image sharing, but we are kind of at the mercy of the platform vendor to implement that option. It looks like another one of the vendor's customers submitted this as an idea a few months ago and it's "acknowledged" right now.


If you find my post helpful, please mark it as an "Accepted Solution".

Re: Allow Copy-Pasting Images in messages

Phenom
Phenom

@KatieKing

This is not a new topic.

It was taken up 4 yrs back

https://community.plm.automation.siemens.com/t5/Community-Suggestions/Copy-and-Paste-from-Clipboard-...

Seems it was left open without any conclusion.

 

But glad to know that it is noticed by the platform provider.

 

The current process is not bad at all, especially for forum users who won't insert more than a couple of images in a post and not every post need an image.

This request would come only from a handful of prolific users, especially like me who post a blog article every week which typically contains 10-15 images.

But, this is a good-to-have feature.

 

So I am not hoping even the vendor would assign any kind of top priority,

 

Thanks for following up.