Cancel
Showing results for 
Search instead for 
Did you mean: 

Insert code with mobile phone

Legend
Legend
I don't find any option for insert code for a reply or a question...
I think it would be a good idea
Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com
2 REPLIES

Re: Insert code with mobile phone

Community Admin Community Admin
Community Admin
Hi @mkn, sorry for the delay. The code button is only for desktop primarily because there isn't a large enough use case for people sharing code related to our products on their phones. That, and the fact that 95% of our users are on desktop anyway. Can you give me an example of when you would use this feature?

-Katie

Re: Insert code with mobile phone

Legend
Legend

Hi @KatieKing ,

Just a simple example of code, but not required: 

if {$version == "mobile"} {
	# Code with mobile phone is impossible...
} else {
        # Have fun !!
}

thank you for the last 5 % Smiley Wink

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com