Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with Signatures

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Does anyone seem to have the same issue as I do with people signatures?

Below are some images of what I am seeing.

I am using Firefox as my browser, but I get the same exact issue if I use IE10.

 

Having used the signatures on the BBS to put relevant information was quite handy, but in Community it looks like we are being limited in how much information we can post.

 

2014-04-24_11-06-06.jpg

 

2014-04-24_11-08-18.jpg

Anthony Galante
Senior Support Engineer
PhoenxPLM
6 REPLIES 6

Re: Problems with Signatures

Community Admin Community Admin
Community Admin

Anthony @PhoeNX_Support -

 

I think this is a pixel setting that I can fix. I will look into that and report back to you on this thread. Thanks for pinting this out. You can use the Community Suggestion thread for any item like this.

 

Thanks!
Susan

 

If you find my post helpful, and it answers your question, please mark it as an "Accepted Solution"

Re: Problems with Signatures

Community Admin Community Admin
Community Admin

@PhoeNX_Support - Moved this post to the Community Suggestion area as it is more appropriate here.

 

There is a pixel height allowed in Signatures. I've increased it. If you find that the increase wasn't sufficient, let me know and I can adjust again. 

 

Thansk!
Susan

 

If you find my post helpful, and it answers your question, please mark it as an "Accepted Solution"

Re: Problems with Signatures

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Susan,

signatures are also including information about the environment one is working in.
This is not displayed here even if it is included in the signature.

In addition I was able to change the size of this environment information to a small font, so it doesn't occupy too much space, but I can't do this here.
I noticed that UBB-code is not supported but HTML tags are, but the style attribute for a paragraph is not supported.

See my signature as an example:

Stefan Pendl

Systemmanager CAx
HAIDLMAIR GmbH - <a href="http://www.haidlmair.at/">http://www.haidlmair.at/</a>

<p style="font-size:small">Windows 7 x64 SP1
Production CAD: NX8.5.3
Production CAM: NX8.5.3, VERICUT 7.3
Production Shop Floor: NX8.5.3 and FBM
Production PLM: TcUA 8.3 MP3 Patch 9 (8.3.3.9), TcVis 10.1
Testing: NX9.0, NX10.0
HP Zxx0/Zbook, 4-64 GB RAM, nVIDIA Quadro FX 4000/1x00 (AMD FirePro V7900/W7000)</p>

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Problems with Signatures

Gears Phenom Gears Phenom
Gears Phenom

This is what I came up with to try and fit my signature in the allowed space:

<b>Graham Inchley</b> Systems Developer, <a href="http://www.sandvik.com/en/">Sandvik Coromant</a>
<blockquote>HP EliteBook 8760w, Win7, 8GB. <i>Developing in</i>: Java | C | C# | KF
<i>Production: </i>NX6.0.5.3 MP5
<i>Testing: </i>NX8.5.2.3 MP0 32bit | NX8.5.3.3 MP4 64bit | NX9.0.2.5</blockquote>

 

Graham Inchley Snr R&D Engineer (Systems Development), Sandvik Coromant
Dell 7530 Precision, Win10, 32GB. Developing in: Java | C | KF
Production: [NX12.0.2 MP1]

Re: Problems with Signatures

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Thanks for the hint with the quote, now everything seems to fit in there nicely Smiley Wink
Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Problems with Signatures

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
using your advice I've now got our video link logo working in the signature. Shame about the height restriction for signatures, but then again, it's easy to get very silly with them.
Anthony Galante
Senior Support Engineer
PhoenxPLM
Try Solid Edge for free