Cancel
Showing results for 
Search instead for 
Did you mean: 

Quick Reply Functionality

Phenom
Phenom

Is it confusing for anyone else when submitting a quick reply does not reload the page with your post present? I always have a few seconds of terror and confusion before I notice the little grey box that says my post was successful. Why not simply update the page to show my reply?

-Dylan Gondyke
4 REPLIES 4

Re: Quick Reply Functionality

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I agree Dylan.
It must be something to do with not loading into the full editor for the post....but, as you suggest, how hard would it be to include the "go to post" functionality so that you're "automagically" transported to where you need to be.

Which reminds me....there needs to be [when in Quick Reply] an "Switch to Advanced Editor" [like there is in the BBS], in case, like I'm doing now, you start waffling on, and lose sight of any kind of format, spelling or gramatical corrections.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Quick Reply Functionality

Phenom
Phenom

Ctrl+A, Ctrl+V has been my "Transition to advanced" button for a while...  Smiley Tongue

-Dylan Gondyke
Highlighted

Re: Quick Reply Functionality

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Chally72 wrote:

Ctrl+A, Ctrl+V has been my "Transition to advanced" button for a while...  Smiley Tongue


Haha....of course, this is how I am forced to do this also....such rebels!

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Quick Reply Functionality

Community Admin Community Admin
Community Admin
Sean - this is a great idea. Let me see if it's a simple checkbox to allow this or not.

Thanks,
Susan
(using the Quick Reply to test Dylan's initial post)
If you find my post helpful, and it answers your question, please mark it as an "Accepted Solution"
Try Solid Edge for free