Cancel
Showing results for 
Search instead for 
Did you mean: 

Side Bar is Awsome

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Perhaps this has been retouched quite some time ago but I just noticed the side bar or side panel on the Solid Edge forum main page looks pretty neat and tidy:

 

sidebarneat.png

   

However I have couple of suggestions:

1. The 'download latest maintt pack' link opens the ST10 page and may need timely attention as new versions are released. If it could be changed to point a level up in the main Solid Edge listing where users can pick their SE version and proceed to pick the latest maintt pack for that version.

    

2. Another blog that can be added is one by David Merritt which though has not been updated since 3-4 years but contains extremely valuable information related to Solid Edge, especially SE administration which is still relevant and useful, especially for those who are still on some older version of Solid Edge  - highly recommended:

   

http//ddavidmmerrittbblogspotin/

   

One more popular Solid Edge blog missing from the list is from Design Fusion:

http://www.designfusion.com/blog.html

   

Thanks.

Tushar

 

5 REPLIES 5

Re: Side Bar is Awsome

Community Admin Community Admin
Community Admin

Re: Side Bar is Awsome

AmyReyes1
Retired

Hooray, I am glad you like it! I just updated it sometime last week I think.

 

Thanks @Tushar for the additional suggestions, I'll implement those later today Smiley Happy

 

-Amy


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Re: Side Bar is Awsome

AmyReyes1
Retired

This is done now and implemented in production. Smiley Happy


Community Manager, Solid Edge
Become a Solid Edge Certified pro today!

Re: Side Bar is Awsome

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Wow! what a fantastic update.

@uk_dave to kindly take note Smiley Happy

 

Re: Side Bar is Awsome

Siemens Phenom Siemens Phenom
Siemens Phenom

@Tushar thanks for the plug :-)

 

@AmyReyes1 thanks for the blog add.  Good to finally get the recognition, even if it is after the fact.  Unfortunately my blog is now somewhat stale :-(

Try Solid Edge for free