Cancel
Showing results for 
Search instead for 
Did you mean: 

[6504] Error came while initializing Parquet Reader for path suppliesTo.parquet

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

I have uploaded a time series entry successfully (status: 204). When trying to read the data I get the follwoing error:

 

{
"timestamp": "2019-02-01T17:00:28.968+0000",
"status": 500,
"error": "Internal Server Error",
"exception": "com.siemens.mindsphere.iot.exception.IotException",
"message": "[6504] Error came while initializing Parquet Reader for path suppliesTo.parquet",
"path": "/api/iottimeseries/v3/timeseries/e36ab5372d524855b34e53d7b30d56d4/suppliesTo"
}

 

What does this mean?

2 REPLIES

Re: [6504] Error came while initializing Parquet Reader for path suppliesTo.parquet

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Update: In the meantime I have done some tests. It seems that the error is due to one variable being of type BIG_STRING. I don't get this error with a variable of type STRING. 

Re: [6504] Error came while initializing Parquet Reader for path suppliesTo.parquet

Siemens Pioneer Siemens Pioneer
Siemens Pioneer

Update: Problem seems to be solved with recent MindSphere update