Cancel
Showing results for 
Search instead for 
Did you mean: 

Create MindConnect Nano Asset via Api's

Experimenter
Experimenter

Hello Community,

 

I try to set up an Asset with the typeId "typeId": "core.mcnano" via the Api's (Asset Management Service, Agent Management Service, Mindconnect API) and Postman.

My Problem is to give the unique identifier of the hardware via the Api's. In which API and Param do i have to configure this ?

 

Additionlly, when i try to do it manuelly i fetch an error: 

500: Interner Serverfehler
An error occurred while creating agent on AgentManagement
 
regards,
PHmind