Cancel
Showing results for 
Search instead for 
Did you mean: 

Data Upload MindLib

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hey,

 

I heard with the summer release it will be possible to send other data structures than float, boolean and string variables to MindSphere.

So I saw that this is not possible to choose something else (than float, boolean and string) with Mind Connect Nano. But is it possible to define own data structures with the MindLib?

 

 

2 REPLIES

Re: Data Upload MindLib

Community Manager Community Manager
Community Manager

Hi @SabineZ, the selectable data types will be the same with the Lib but the Lib offers you a Blob upload with which you could basically upload any data type into MindSphere, you then merely need to create a custom parser.

If you are a MindDeveloper, you also have access to the SIOS extranet where the MindConnect Lib documentation is stored. You can find further extensive insights into the Lib there.

Please let me know if you have any further question.

David

Re: Data Upload MindLib

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

How do you retrieve blob data via the MindSphere APIs?