Cancel
Showing results for 
Search instead for 
Did you mean: 

connecting nano to single device

Hi,

 

Nano and IoT2040 supports OPCUA and S7 protocol.

 

But if I have a requirement to connect single motor with few sensors. Is there any other way to collect dat and send it to Mindsphere using nano? Or do I need to configure entire OPCUA or S7 for this?

 

Thanks,

Prashant

1 REPLY 1

Re: connecting nano to single device

Experimenter
Experimenter

Mindconnect Nano and Iot2040 support S7, OPC UA, Modbus Tcp, Modbus Rtu, IOshield protocols. The only way of reading some data and uploading to Mindsphere is using one of these protocols.