Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: [dataexchange API] Using the filter param when listing directories

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

 

The behavior of filter param is not consistent. Sometimes it gives errors.

For example if the directory is empty and we use the below API, it gives intermittent errors: 

https://gateway.eu1.mindsphere.io/api/dataexchange/v3/directories/2cbc06e5-2b86-485c-af4b-5cf80e45bc...

 

{

    "errors": [

        {

            "code": "mdsp.core.dataexchange.exception",

            "logref": "e1b682fde91d47a38175ddc687eb119d",

            "message": "There was an internal error. Please retry or contact the support if the error persists."

        }

    ]

}

Is this a known issue ?

 

Regards,

Sandeep 

 

Re: [dataexchange API] Using the filter param when listing directories

Experimenter
Experimenter

Hi,

 

this is indeed correct. We've replicated this as well, so we're looking into it.