Cancel
Showing results for 
Search instead for 
Did you mean: 

10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer
have a proven UG-Post wrote new in 9.0.2. using everyday. M11 and M10 out properly when I open up the post and make no changes - save it in 10.0.3 then try using it - I receive the error code "1770002" ?? when looking in my log file I see that the problem is around Auto Clamp ***TCL_ERROR***: Event Handler: C:\Users\a........-Makino-nx10.tcl, Event: MOM_before_motion, Error: invalid command name "AUTO_CLAMP" while executing "AUTO_CLAMP" (procedure "PB_CMD_kin_before_motion" line 57) invoked from within "PB_CMD_kin_before_motion " (procedure "MOM_before_motion" line 17) invoked from within please advise, thank you.
8 REPLIES

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Which controller template is used? Looks like something wrong with the template post.

 

Li Li

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer

not sure exactly what you mean by controller template ---

 

but i am using exisitng clamp info supplied from the installation: ----

 

#
#  This procedure is used by auto clamping to output the code
#  needed to clamp the fourth axis.
#
#  Do NOT add this block to events or markers.  It is a static
#  block and it is not intended to be added to events.  Do NOT
#  change the name of this custom command.
#
  MOM_output_literal "M10"

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Post Builder ->File->post properties

you will find below controller family and controller template post directory

 

pb_template.jpg

Li Li

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer

Standard Fanuc - 1030i

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer
I can't past the screen shot for some reason - please see attached

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer

worked fine in NX9.0.2 - --

 

not so when saving into 10.0.3

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Before you get too far, did you update PostBuilder with patches?

There were several issues in the original 10.0.3 version that were fixed.

 

Either update to the latest 10.0.3 MP or see the patch instructions in SFB-NX-9430. 

 

 

 

 

Mark Rief
Retired Siemens

Re: 10.0.3.5 Post Builder - Auto Clamp ??

Pioneer
Pioneer

Thanks Mark, downloaded and installed MP02 for NX10.0.3 and it took care of the issue.

Learn online





Solution Information