12-11-2017 06:57 AM
Hello,
-I had turned on 2D dynamic in NX11.0.2.7 and now I see that it doesnt show the simulation.
-The same in NX12
-Customer gets in NX11 customization an error: wrong camipw library.
It is some well know problem/status or do I have something wrong with my PC?
thank you for help
12-11-2017 07:47 AM
I tested it in my installed NX12.0 and do not have any problem.
12-11-2017 09:05 AM - edited 12-11-2017 09:07 AM
hi,
I attached log file and video
12-11-2017 09:33 AM
Hello as I do not see any error message, but also no material removal in the graphics, I can not give any further hint. The problem may lead to a known limitation about a graphics card setting. Please search the Forum about that, there are several message about that, I do not have details.
May I allowed to ask why 3D is not sufficient for your customer?
12-12-2017 08:16 AM
hello,
(funny is that 2d worked some time before on my PC. Also on my colleauge 2d dynamic doesnt show simulation)
Customer said that 2d is faster and looks better
12-12-2017 01:54 PM
I had this issue and went into the C:/users/yourlogname/AppData/Local/Siemens folder.
Rename the The NX110, or the NX120 folder. Relanch NX and it will create a new folder.
All settings will be "out of the box" again.
If this doesnt solve it, delete the new folder and rename your back to revert everything.
I usualy save a "role" with my settings before, and just copy the roles fodler into the newly created folder. I then apply the role to get my settings back.