Cancel
Showing results for 
Search instead for 
Did you mean: 

3D DYNAMIC DISPLAY

Pioneer
Pioneer

Hello all,

Q. When using the 3D Dynamic display of the toolpath.

Is there a way so NX always only shows the part and the current IPW.

All other geo would be hid.

Returning all to show when going out of it.

 

Not sure if I am explaining this correctly.....

Out side of turning off all levels with geo before hand....

 

I am now in 11.0.2.7

2 REPLIES 2

Re: 3D DYNAMIC DISPLAY

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

as far as I know there is no automatism function doing that for you, when enter and leave 3D verify.

Sorry.

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: 3D DYNAMIC DISPLAY

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could possibly Menuscript a /PRE and /POST action?

You would have to figure out the "action" of going into (3d) Verify (go into in then look at the syslog/NX Log file to see what the "action" is)

Then do the Menuscript to have an application specific over-ride of that action.

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information