Cancel
Showing results for 
Search instead for 
Did you mean: 

3D Profile Under Ledge

Experimenter
Experimenter

I have a part that I am cutting using a form ground slot mill that makes a shape on the bottom of a ledge.  I would like to approach at an upward angle and retract downward but using a negative value in Z has no effect. Any suggestions?  The toolpath is generated using 3D Profile and I am following a spline around the part. 

4 REPLIES 4

Re: 3D Profile Under Ledge

Legend
Legend

I'm not sure I understood your question, but maybe you could use Start and Return points in Avoidance section of non-cutting moves.

 

avoidance.JPGhope this helps

ciao

Re: 3D Profile Under Ledge

Experimenter
Experimenter
I did try as you suggested, but the engage and retract are still starting and ending the cut in a planar move. I was hoping for a 3D style of ramp feeding into the cut, and the same for retract.

Re: 3D Profile Under Ledge

Legend
Legend

if engage and retract ramps have to be linear you could use linear along vector as engage and retract methods.

if they are not linear I'm afraid you have to change operation type, for example you could use fixed contour with a drive curve comprising engage and retract path.

Re: 3D Profile Under Ledge

Experimenter
Experimenter
That is what I needed. Thanks

Learn online





Solution Information