Cancel
Showing results for 
Search instead for 
Did you mean: 

4-5 axis with file .STL.

Pioneer
Pioneer

Now, i am researching run 4-5 axis with file .STL. Anyone who has ever done this not?

14 REPLIES

Re: 4-5 axis with file .STL.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I have researched this question in past...

Re: 4-5 axis with file .STL.

Pioneer
Pioneer

Yes, this is

How do you way?

I can not to do it, Can you help me?

Thanks

 

Re: 4-5 axis with file .STL.

Legend
Legend
CuongVo, unless your machine tools are bench-top's $2000 worth each, then you can quickly rig together some NXOpen classes using CAM.path and some point3d/vector3d transformations for machining any irregular shapes, facets, whatever really.

From previous experiences with these sort of nxopen plugins, it works one time on two. Perfect if you have time to waste sitting in front of a computer screen all day long then that might become a new hobby that you'll like.

If for a production/engineering environment, my advice is to learn about the NX's Reverse Engineering and Surfaces tools before. Working with well defined geometry from the start makes things simpler (and much cheaper) at the end of the day.

Re: 4-5 axis with file .STL.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Attached find a vb journal with block dialog to create faces from facets, it can take quite some time if there are hundred thousand facets.

  1. Import the STL into NX
  2. select the faceted body and the process parameters
  3. OK and wait for the process to finish

This is only tested with NX 10.0.3.

 

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: 4-5 axis with file .STL.

Pioneer
Pioneer

Thank you so much!

I am personal research because passion. I am living in Viet Nam. In here, very low income so i has not money to learn the course such as you tell with me.

Once more thank you!

Re: 4-5 axis with file .STL.

Pioneer
Pioneer
Thank you!

I am finding way to use file you send. If you have questions I will contact you

Thanks so much!

Re: 4-5 axis with file .STL.

Pioneer
Pioneer

You can guide me to add (install) this StlToSolid into NX?

I don't know way to intall this file into NX.

Thanks!

Re: 4-5 axis with file .STL.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The VB journal can be in any place.

The DLX file must be in an application sub-folder pointed to by the variables UGII_SITE_DIR, UGII_GROUP_DIR, UGII_USER_DIR or any folder contained in custom_dirs.dat

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: 4-5 axis with file .STL.

Pioneer
Pioneer

Hi Stefan_Pendl!

 

Excuse me! can you create a video guide for me?

I don't never install add-in such as this in NX so don't understand way to use in NX.

Thanks so much!

Learn online





Solution Information