Cancel
Showing results for 
Search instead for 
Did you mean: 

4th axis C table not allowed

Experimenter
Experimenter

Hey guys,

 

we have the post processor for a Deckel FP4 in our company. But when I open it, it's completely set up for 3 axis milling. Our machine has an additional 4th C axis, which I try to implement by making a new post based on the old one and the machine tool setting 4th axis with rotary table. When I choose the plane of rotation XY inside the postbuilder 8.0, i get the error: 4th axis C table not allowed. The other two axis would work fine but are useless for me.

 

Any ideas what I'm doing wrong?

 

Regards,

Bernd

2 REPLIES

Hi Bernd,   A colleague offers this answer: >>>>> The C-a...

Community Manager Community Manager
Community Manager

Hi Bernd,

 

A colleague offers this answer:

>>>>>

The C-axis is a redundant axis in this configuration and would have an infinite number of solutions for each position.

In principle the C-axis will not do anything unless the Rotate UDE is used.

 

Another alternative is to use the “3-axis Mill-Turn (XZC)” post as the solution for using the C-axis instead of Y-axis. However this configuration is not supported by any of the Sinumerik Controllers. The code for translating XYZ into XZC is fairly simple though.

He might need to swap the post, based on what he wants to do with it.

 

His choice will depend on what he wants to accomplish with that rotary axis. He can’t use the all 4 simultaniously.

<<<<<

 

Hope this helps.

Derek Hart
... if we're not having fun, we're not doing it right!

Hello NXBernd - did Derek's response answer your question?

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Hello NXBernd - did Derek's response answer your question?

Make Better Parts Faster!
Aaron Frankel (Community Manager)

Learn online





Solution Information