Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: 5-axis Machining

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Why does it seems I'm missing that operation?

12.JPG

Highlighted

Re: 5-axis Machining

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You seem to have NX 12.0.0 instead of NX 12.0.1 installed.

Note that starting with NX 10 or even NX 9 new features are added in MRs too, the base release is mostly resembling the stage of the last previous release.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: 5-axis Machining

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, Guiding Curves for Multi Axis is available in NX12.0.1

Lead Product Manager - Mold & Die

Re: 5-axis Machining

Solution Partner Creator Solution Partner Creator
Solution Partner Creator
Sir, where can I download the maintenance pack for 12.0.1? GTAC download site is not loading when search tab is used.

Re: 5-axis Machining

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Go to http://siemens.com/gtac/ and select the section "download and upload files", enter your webkey credentials, select "NX => product updates => maintenance release => NX12 => platform", download the file nx-12.0.1.r1.README.TXT first and read through it. Afterwards follow its advice.

In addition read through the thread NX 12.0.1-Maintenance Release Announcement at the NX design forum. Any new release will be announced at the NX design forum, since it is their responsibility.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: 5-axis Machining

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you very much, guiding curves is a big help for my inquiry.

 

Now I'm trying to use guiding curve to this model (attached photo) I kept on getting an error.

 

HEAD.JPG

 

Hope you can also help me with this one.

 

I downloaded the file from https://www.youtube.com/watch?v=j_HimxaZpdI

 

Re: 5-axis Machining

Siemens Phenom Siemens Phenom
Siemens Phenom
Glad that you like Guiding Curves.

If you run into issues, please file an IR with the part and CAM Setup attached.

Thanks in advance!
Lead Product Manager - Mold & Die

Learn online





Solution Information