Cancel
Showing results for 
Search instead for 
Did you mean: 

5-axis Machining

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi Cam masters,

 

I am new with NX Cam, can you guys teach me how to machine the attached photo of an object by a 5-axis machine using nx cam express without using the surface area as drive method. Client wants to know a faster and easier way to machine similar objects as show. Client does not want to make a half sphere just to make it as a drive method.

 

All replies will be much appreciated.

Thank you,

 

pawn.JPG

26 REPLIES 26

Re: 5-axis Machining

Gears Phenom Gears Phenom
Gears Phenom

use streamline,

flow1 - point on surface,on the top,

flow2 -  bottom edge

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: 5-axis Machining

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @ReyL,

 

I would like to advise you to have a look at one of our newest enhancements, which we introduced into NX12.0.1. The Variable Axis Guidung Curves. The Benefit of this new operation type is, that you don't need to define any projection vector and the handling is much easier then with Streamline.

 

Let me guide you step by step on how I would do such a part. At the end of my reply I attached a video with the complete workflow.

 

1. Create a CSYS above the part in the middle, where you can attach your Sketch in 2.

2. Create a Sketch and draw a circle with a small diameter (smaller or equal the Stepover in the operation) exactly in the middle of the part.

3. Project the circle onto the part geometry (see pictures below)

2018-02-22 15_27_37-NX 12 - Manufacturing.png2018-02-22 15_28_43-NX 12 - Manufacturing.png

 

4. Create a Variable Axis Guiding Curves Operation (picture below)

2018-02-22 15_30_29-NX 12 - Manufacturing.png

 

5. Select the cut area 

6. Select the two curves where the operation should morph in between

7. Make your choice of the cut pattern and define the value of the stepover.

8. Define the Tool Axis with Away from Point. Other methods can also be done, but this is my prefered one because easy to handle and avoids to create drive geometry etc.

9. Generate and review your toolpath :-)

 

(view in My Videos)

 

If you have any further questions, please let us know.

 

Cheers,

Alexander

 

Lead Product Manager - Mold & Die

Re: 5-axis Machining

Gears Phenom Gears Phenom
Gears Phenom

I can say that guiding curves is quite good new drive method. We can drive cut pattern,I have to say good job.

But in this case, streamline has less clicks than guiding curves, so streamline could be a bit faster.

->Specify 1 point as a flow1  and  2nd flow as down edge

+ projection vector

+tool axis

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: 5-axis Machining

Siemens Phenom Siemens Phenom
Siemens Phenom

Played around a bit with Variable Axis Guiding Curves. I have another workflow, where you don't need any geometry creation or Tool Axis selection. So this is a very fast way programming and a beautiful toolpath as a result.

 

Only choosing one Guide curve and pattern type Constant Offset (picture below)

2018-02-22 16_53_44-NX 12 - Manufacturing.png

 

Using Fixed as Tool Axis and Tilt/Retract as the Avoidance option (picture below)

2018-02-22 16_57_33-Variable Guiding Curves - [VARIABLE_AXIS_GUIDING_CURVES_1].png

 

Also made a video showing this workflow:

(view in My Videos)

 

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: 5-axis Machining

Gears Phenom Gears Phenom
Gears Phenom

this is nice, just put there some helical pattern and done .

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: 5-axis Machining

Siemens Legend Siemens Legend
Siemens Legend

Helical will be released in 12.0.2, but is available under ENV. send me a private mail (eddy.finaro@siemens.com) and I can share the ENV with youSmiley Happy

 

Yours

Eddy Finaro
NX CAM Product Manager
Siemens PLM

Re: 5-axis Machining

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The guided curves drive pattern has the potential to eliminate many undercut troubles Smiley Wink

Thanks @Eddy_Finaro and your team.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: 5-axis Machining

Gears Phenom Gears Phenom
Gears Phenom

Hi @AlexanderFreund

I remember I have simillar test part.

I was trying to set operation in the same way.

I generates path in few seconds but still "work in progress" path disappear and take time

So I canceled the calculation.

See attached part.

Did I make a mistake?

 

/

When I made this part bigger (ball diameter 125mm, error was returned - some library failure)

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: 5-axis Machining

Siemens Phenom Siemens Phenom
Siemens Phenom
Can you file an IR to GTAC?

Can't see the part attached.

We are currently working to enhance the Performance of the Tilt Tool Axis functionality
Lead Product Manager - Mold & Die

Learn online





Solution Information