Cancel
Showing results for 
Search instead for 
Did you mean: 

5 axis drilling_ transfer

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi.

In my part, I create a drilling operation. My holes are placed in two different places.

The first hole is B0.

The second hole is B180.

 

But in the post, I have a lot of B value because of non-cutting transfer.

I want indexable move. First Z Y second B axis move. Like canned drill cycles

How I solve this problem?

My machine is a horizontal machining center.

b axis.JPG

2 REPLIES 2

Re: 5 axis drilling_ transfer

Phenom
Phenom

Hi @Batigol ,

It's coherent with your cls file , I would do :

2 operations

or

1 operation but for the first hole I would do with a large retract and I would delete the part in workpiece too

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com
Highlighted

Re: 5 axis drilling_ transfer

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

My workpiece is now empty.

I do clearance option is Sphere and I generate the tool path so now I have Simultaneous motion. This is not for me.

My claim is indexable motion like this 

G0 Z50;

G0 B180;

G0 X20 Y20;

G81 ......

That I know If I create two operations for two faces we will see only B180 and B0

 

 
cc.JPG

Learn online





Solution Information