Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

A C two head rotary ,initial angle is different from motion angle?

Pioneer
Pioneer

Hi everybody,

 

I have a new 5-axis milling machine (AC-head) in heidenhain, with C-stroke +90  -270.

 

I do a programe on 5-axis. the initial angle  is C 90,  the motion angle C-269.879. 

 

the positon c90 and c-270 is the same .

 

I want to change initial angle is C-270,  how to do?  I attack file with the part and postprocessors.Capture.PNG

 

 

Thank you in advance

Production: NX 11.0.2.7 MP10,

2 REPLIES 2

Re: A C two head rotary ,initial angle is different from motion angle?

Legend
Legend
You can set the initial angle with the UDE Rotate

regards

Re: A C two head rotary ,initial angle is different from motion angle?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

as @schauerm3 mentioned -  use ude rotate

 

I tested your case with ude rotate set as bellow

aa.JPG

19 L A-45. C-270. FMAX
20 L M128 F1000.
21 L X-1199.974 Y7.882 Z34.149 A-45. C-270. FMAX
22 L X-1009.734 Z-156.091 FMAX
23 L X-929.651 Z-236.174 F200.
24 L X-928.777 Y7.788 Z-237.048
25 L X-927.924 Y7.501 Z-237.9
26 L X-927.112 Y7.029 Z-238.71
27 L X-926.363 Y6.384 Z-239.457
28 L X-925.694 Y5.581 Z-240.124
29 L X-925.122 Y4.64 Z-240.693
30 L X-924.66 Y3.585 Z-241.151
31 L X-924.321 Y2.44 Z-241.486
32 L X-924.113 Y1.236 Z-241.691
33 L X-924.04 Y+0.0 Z-241.76
34 L X-924.03 Y-2.962 C-269.816
35 L X-924.021 Y-5.924 C-269.633
36 L X-923.992 Y-8.886 C-269.449

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information