Cancel
Showing results for 
Search instead for 
Did you mean: 

A CSE question?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello, I have a machine and simulate machine code file:

PLANE RESET STAY
M129
TOOL CALL 1 Z S6000 DL0.0
CYCL DEF 247 DATUM SETTING Q339=+1    ;DATUM NUMBER
PLANE SPATIAL SPA0.0 SPB-37.38 SPC72. TURN FMAX SEQ+
L X0 Y0 Z0 F1000

 

Result is:def247.png

I would like to make tool position to go to MCS(0,0,0). How can I do it?

7 REPLIES 7

Re: A CSE question?

Gears Phenom Gears Phenom
Gears Phenom

As I see on right picture you already are on x0y0z0. It is OK. Machine did it correctly.

Actual active MCS is in the midle of purple face.

This is how tilded plane works. Zero point is where it was indicated, only direction is changing.

But in this case we dont see this transformation.

 

If you mean 000 on highlited mcs on the right picture you have to disable plane or tcpm.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: A CSE question?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thank you for your reply.

I am a bit confused. I want to machine the right side of the tool on right picture. NC code like:

L X+44.5073 Y+2.0734
L X+44.5079 Y+2.0734 Z-7.9621
L Z-8.9621 F1000.
L X+36.7579
L X+35.5079 Y+6.9146 Z-8.9622
L X+35.5018 Y+6.9381
L X+31.9036 Y+9.0156
L X+35.5079 Y-4.9439
You can find the face that is under MCS. The NC code is Z-8.9622. If you are right, then NC code Z value should be +Z?.

This becomes a post processor error. But my post processor on CNC is correct.

I have found that the result of the NC code output from my post processor is that the origin of the coordinate will not follow the rotation, but the axis will rotate due to the rotation.

What's this problem? CSE? Post-Processor?

How can I correct it?

 

Sam Huang

 

Re: A CSE question?

Gears Phenom Gears Phenom
Gears Phenom

better will be to attach the part and see operations

now I dont know what you wan to achieve and where is the problem

 

"I want to machine the right side of the tool on right picture"

 

Another thing machine simulation can overide postprocesor kinematics etc

but we dont know if it is a problem in this case.

 

Or there can be problem with zero point settting with cycle 247, dont know. I am not into simulation so much.

 

attach the prt

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: A CSE question?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

See attach part

Re: A CSE question?

Gears Phenom Gears Phenom
Gears Phenom

This is my output:

39 PLANE SPATIAL SPA+14.4888 SPB+34.8393 SPC-83.6611 TURN FMAX TABLE ROT
40 L X-3.6621 Y-1.9307
41 L Z+102.9597 FMAX M3

or this:

41 PLANE SPATIAL SPA+0 SPB-37.3774 SPC+72 TURN FMAX SEQ- TABLE ROT
42 L X+2.7932 Y+3.0556 R0 FMAX M3
43 L Z+102.9597 FMAX

 

as the first point

And the cutting level coordinate is:

L  Z+6.6055 FMAX

L  Z5.6055 F1000

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: A CSE question?

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Dear Juraj,

Thank you very much.

I found the problem!

As you say "another thing machine simulation can overide postprocesor kinematics".

When I load the machine and the post result is (Wrong):

L X+44.5073 Y+2.0734 F5000.
L Z+88.392
L X+44.5073 Y+2.0734
L X+44.5079 Y+2.0734 Z-7.9621
L Z-8.9621 F1000.
L X+36.7579

When there is no machine and the post result is (Right):

L X+2.7925 Y+3.0556 F5000.
L Z+102.9597
L X+2.7925 Y+3.0556
L X+2.7931 Y+3.0556 Z+6.6056
L Z+5.6056 F1000.
L X-4.9569 Z+5.6055

 

 

Re: A CSE question?

Gears Phenom Gears Phenom
Gears Phenom

you can put "return" in "pb cmd reload iks parameters" and you disable that overiding

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information