Cancel
Showing results for 
Search instead for 
Did you mean: 

ADAPTIVE_MILLING generate speed

Valued Contributor
Valued Contributor

Hello,

Please generate the operations in the attached file. When the raw material is full, ADAPTIVE_MILLING and VOLUMIL generate the tool path at about 2 minutes. But when IPW is used for the second operations (SEMI_FIN), ADAPTIVE_MILLING made it in about 3 hours since it took about 3 minutes for VOLUMIL to perform the task for identical settings. However ADAPTIVE_MILLING made a far more better tool path compairing to VOLUMIL.

Am I doing something wrong here?

VOLUMIL uses more than 70% of the CPU while ADAPTIVE_MILLING cannot use more than 25%.

Kind regards

Majid

Majid
6 REPLIES 6

Re: ADAPTIVE_MILLING generate speed

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

send it to gtac, it is poor.  cavity can handle that rest machining it in a minute

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: ADAPTIVE_MILLING generate speed

Valued Contributor
Valued Contributor

And how I send this to GTAC?

We are NX user (Germany)

Majid

Re: ADAPTIVE_MILLING generate speed

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

you have account here soyou should be able to log issue / ticket on GTAC.

https://www.plm.automation.siemens.com/global/en/support/

or contact your support, they will help you

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: ADAPTIVE_MILLING generate speed

Siemens Genius Siemens Genius
Siemens Genius

Help --> Online Technical Support --> Log an Incident with Technical Support.

Best regards

Lars Okkels
Siemens, MBG

Re: ADAPTIVE_MILLING generate speed

Phenom
Phenom

Try creating a cylinder as geometry and pick that as your stock. When using the automatic bounding box and cylinders in "workpiece" as stock, I have had nothing but problems with generation speed.

 

The last op in P2 was still taking a lot of time. I let it run for about 20 min and had to kill it. It did not seem to freeze though, the "Pattern creation" numbers kept changing. See if it works better for you. 

 

 

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: ADAPTIVE_MILLING generate speed

Valued Contributor
Valued Contributor

Glen, It did not help.

 

And I could not send the issue to GTAC. The portal said I have to contact the local distributor first, then they will see if they can solve (which I am sure they can not) then they will contact ...

 

Since it is a general problem, can anyone kindly send a ticket for that and inform us all about the result?

 

Best regards,

Majid

Majid

Learn online





Solution Information