Cancel
Showing results for 
Search instead for 
Did you mean: 

Active error "standard C++ exception caught. See system log for details"

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hi

 

OS : Window7 64bit

Version : NX9.0.3.4_MP9_hf62

 

error message : standard C++ exception caught. See system log for details

 

error.gif

 

it's activated when the operation generate.

 

What is the error?

3 REPLIES 3

Re: Active error "standard C++ exception caught. See system log for details"

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi.

 

Looks like PR, which I reported.

Error appears when you choose Verify directly from CAM operation window.

As a workaround you should be able to start Verification from menu button.

 

Should be fixed in NX9.0.3 MP11

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Active error "standard C++ exception caught. See system log for details"

Please log a call with GTAC so  they can verify this and document your use case.

It could be a completely different problem.

Mark Rief
Retired Siemens

Re: Active error "standard C++ exception caught. See system log for details"

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

This was reported on PR 7540587

( problem is in NX 9.0.3 MP9)

Verify may show an C++ Exception when leaving the dialog with OK and Verify has been called from the oepration edit dialog. This will be resolved by code changes made to the release of our product NX 9.0.3 MP11

( not a problem in NX 10.0.2 MP3)

 

As MarkR says, you may be seeing a different problem if the errors results from generating an operation.

Learn online





Solution Information