Cancel
Showing results for 
Search instead for 
Did you mean: 

Adaptive Machining Question

Legend
Legend

I'm sending some adaptive to the floor for the first time. I always thought the green lines were traverse motions.

I should be able to override the traverse feedrate, but it is having any effect.

So... I seem to be cutting a bunch of air at metal cutting feedrates.

I did a list tool path and did not see feed changes so It does not look like a post issue.

 

Addaptive image.png

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

3 REPLIES 3

Re: Adaptive Machining Question

Legend
Legend

Those are stepover motions.you can change their feedrates.Look at jpeg file!

-----------------------------------------
NX 12.0.2.9 MP5 / Testing NX 1847
CanikSoft NC Post-Processing & G-Code Simulation
www.plast-met.com.tr
www.caniksoft.com

Re: Adaptive Machining Question

Legend
Legend

Excellent, Thankyou

{Paul Schneider}, {CNC Programmer}, {DRT-Rochester}


Production: {NX11.0.2,MP5, NX12.0.2, MP4}

Re: Adaptive Machining Question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you want to know what motion type is what color, 

In the operation -> Options block -> Edit display -> Path display Colors

 

The only issue is that (OOTB) Siemens uses the same color (blue) for several motion types

 

If you want to change the colors, this can be done in the method view parent methods (or the operation)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information