Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Add Code set in ISV.

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

#Infomation

Version : NX11

Controller : Hei530

Machine Type : Head-Table(AC)

 

# Request

 

How to set up unconfigured code G75.

When you start the simulation, the following message will be activated.

 

22.png

 

 

How do I setup?

 

 

3 REPLIES

Re: Add Code set in ISV.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

you need the Machine Configurator to add the metacode to MCF/CCF file.

 

How to do this? --> look at the available TechTips about Machine Tool Simulation in NX

https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX/Customize-Your-Machine-T...

 

 

Thomas

Re: Add Code set in ISV.

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

I set the G75 Code. 

However, it seems that an additional error message is caused by a code problem in the same block.

 

1111.jpg

2222.jpg

 

I do not know what to add. What is the method? help me...please

Re: Add Code set in ISV.

Siemens Phenom Siemens Phenom
Siemens Phenom
Where have you defined the FP variable? If it´s not defined you can do this in two ways
1. Using NC Code Sinumerik variable definition e.g. DEF NCK INT FP
2. Add FP as variable in Machine Configurator (Variables Tab --> System Variables --> Global variable (channel independent) or Variables (channel dependent))

Thomas

Learn online





Solution Information