Cancel
Showing results for 
Search instead for 
Did you mean: 

Add Operations in Planner_Mill

Pioneer
Pioneer

i added operatinns in planer mill and changed their nanes., when i go to work with them,the change of names doesn"t work.

I add photos .

thank"s for help.

 

Amnon

8 REPLIES

Re: Add Operations in Planner_Mill

Genius
Genius

Hello,

 

Are you using the updates folder? did you make the changes to the planar_mill in there or in a custom enviroment?

 

If you have the option use latest templates then if the Update folder contains the same base option it will use that not the one in the templates location.

 

Hope this is of some help.

 

 

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Add Operations in Planner_Mill

Pioneer
Pioneer

Hi Dave

i made the changes in the Mill_Planer File.

regards,

 

Amnon

Re: Add Operations in Planner_Mill

Genius
Genius

Hi Ammon,

 

There are two locations that could have the same file in it the main location would be C:\Siemens\NX10\MACH\resource\template_part\metric

And the other is

C:\Siemens\NX10\MACH\updates\template_part\metric

 

If you changed the file in the main location this will be cancelled out as it will pull the one from the updates location unless you turn off use latest templates.

 

 

Regards

Dave
NX10.0.3MP13
NX11.0.1
Production
TC10
Vericut 7.3,7.4.1,8.0.2

Re: Add Operations in Planner_Mill

Pioneer
Pioneer

Hi

in "updates" i saw the new operations.is this fine?

 

regards,

 

Amnon

Re: Add Operations in Planner_Mill

After you create an operation, go to Menu > Information > Part > Loaded Parts, and verify where the template part is located.

You should not modify files in the updates area - this is for Siemens to provide updated template and library files in a maintenance release or maintenance pack.

You should create a copy of the mill_planar template part and modify that. See these tech tip videow for one way to do this:

Getting-started-with-NX-CAM-customization

How-to-create-a-NX-CAM-custom-operation-template

I would not rename the out of the box operations. Instead, copy and paste one, rename the copy, and change the template setting on the original so that it cannot be used as a template.

Mark Rief
Retired Siemens

Re: Add Operations in Planner_Mill

Pioneer
Pioneer

Thank you Mark

i"ll try to do the customs like in the links you sentHeart

regards,

 

Amnon

 

Re: Add Operations in Planner_Mill

Pioneer
Pioneer
Hi Mark
can i get pdf of the 2 videos?
thank you

Amnon

Re: Add Operations in Planner_Mill


@Amnon wrote:
Hi Mark
can i get pdf of the 2 videos?
thank you

Amnon

I attached pdfs of the presentation slides to each of the tech tips.

There are no pdfs of the demonstrations.

 

Mark Rief
Retired Siemens

Learn online





Solution Information