Cancel
Showing results for 
Search instead for 
Did you mean: 

Additive Operation MOM_variable

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

hello...Smiley Happy

 

I'm developing some parts of Post.

 

However, the functions in the Additive Operation cannot find or find Path Overhang's Mom_Variable in Debug Mode.

 

Is there a way to print the following part from Post?

 

Overhang.jpg

2 REPLIES 2

Re: Additive Operation MOM_variable

Siemens Phenom Siemens Phenom
Siemens Phenom

What application are you using to make the postprocessor? Is it Post Builder or Post Configurator?

You can use the Review Tool in either case to see the available mom variables and their values with each MOM event. Set Review Tool to On at the bottom of the Postprocess dialog when posting tool path.

If you are using a Full license of Post Configurator, you can see a similar, more detailed view using the Inspect Tool in the debugging options.

Re: Additive Operation MOM_variable

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

thank you for reply....Smiley Happy

 

I used debuging mode... .but not find overhang mom_variable..

 

Is the Operation still owned by the DMG?

 

 

Learn online





Solution Information