Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Additive manufacturing

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I want to check if NX12 able to do layer deposition using Cam command ? Machining is from top down . While additive is bottom up . If We could reverse the programming from bottom to top ?

 

 

12 REPLIES 12

Re: Additive manufacturing

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Edwin_DTS

You can reverse the program from the Tool Path Editor. That will make a top down operation bottom-up.

2018-06-21 14_17_28-NX 12.0.1.7 - Manufacturing.png

Paul

Re: Additive manufacturing

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks Paul . It Helps .

Re: Additive manufacturing

Siemens Genius Siemens Genius
Siemens Genius

Did you try Multiaxis Deposition. It is in NX12 and it is for additive manufacturing.

 

There are some cases where we could not sell it, but for FDM, I think that we can.

Re: Additive manufacturing

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

HI Javi ,

 

I could not see any command in NX12.0 for additive manufacturing . Is there any additional installation ?

May i know what FDM mean /

 

Edwin

Re: Additive manufacturing

Siemens Genius Siemens Genius
Siemens Genius

Edwin,

 

If you create a new part, then you have a template for that. I have NX12.0.1 and I see this.

multi.jpgI also have a template for it when creating a new operaton
multi2.jpgDon't know if it is related to the license...

 

FDM stands for Fuse Deposition Modeling and it is the technique that most of 3D printers use for plastic parts. Also 3D printers for home use are FDM.

Re: Additive manufacturing

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Javi,

 

I think yours have special installtion or special license . I can see it in template but not multi axis deposition. If you have any idea how it work . you can let me know .

 

Best Regards,

Edwin

Re: Additive manufacturing

Siemens Genius Siemens Genius
Siemens Genius

Hi Edwin,

 

I'm 100% sure that I have an OOTB installation. The only difference is that I'm using an internal SIEMENS license.

Anyway, I think that this will be released in August with some  llimitations.

Re: Additive manufacturing

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi Javi ,

 

I am using Partner license . I hope it can work . Thanks for the Info .

 

Best Regards,

Edwin

Re: Additive manufacturing

Siemens Creator Siemens Creator
Siemens Creator
There is a NX Multi-Axis Deposition package either as an add-on to an existing NX seat, or as a complete CAD/AM seat.

It is available today for FDM and non-hybrid wire feed machines. When people are referring to August, that is when some contracts expire, and we can provide a blown powder and hybrid metal solutions.

What type of additive manufacturing machine do you have?

Learn online





Solution Information