Cancel
Showing results for 
Search instead for 
Did you mean: 

Advantage script how to operate registry in the tcl

Pioneer
Pioneer

dear all

 

i want to read&write vaule from the registry , can you give me a simple example?

2 REPLIES

Re: Advantage script how to operate registry in the tcl

Esteemed Contributor
Esteemed Contributor

If you are trying to interact with the registry in tcl, I would search the web.  I Googled "tcl read windows registry" and saw a number of likely links.

You may need to run a separate tcl instance that has registry functions available.

If so, check out the file %UGII_BASE_DIR%\POSTBUILD\pblib\custom_command\pb_cmd_ugwish_win64.tcl

for the "correct" way to spawn another process and have the post wait for it to finish & return data.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Re: Advantage script how to operate registry in the tcl

Legend
Legend

Have you looked this adress http://wiki.tcl.tk/1264 proposed by @MarkRief ? topic by you... post how to operate registry

 

Ihmo , for questions in pure tcl , you should ask here

@mkn
Production: NX11.0.2.7,VERICUT 7.3.3
Development: Tcl/Tk, Gnuplot
www.deshors-tiremold.com

Learn online





Solution Information