Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: After NX 9.0.2 version Z level problem

Valued Contributor
Valued Contributor

i tired extend the path at the edges . it's working if i write 10mm . 

But for 2 mm ; same problem . Smiley Happy

 

Highlighted

Re: After NX 9.0.2 version Z level problem

Valued Contributor
Valued Contributor

Thank you so much friend.

 

i just saw your part. yes , i tired to do this .

But change your tool for example 4mm , it doesnt work friend. 

Re: After NX 9.0.2 version Z level problem

Legend
Legend

Alican,

since you are going to trim the path, it you can extend it as much as you want, so why limit the extension to 2 mm?

After extending  at edges, you have to redefine cut levels top  and depth of range since cut levels adapt to extended cut area.

 

Have you also tried increasing merge distance?

Cattura4.PNG

ciao

 

 

Re: After NX 9.0.2 version Z level problem

Legend
Legend
i tried changing tool diameter to 4,3,2 mm, using the part i sent and it worked all the times

Re: After NX 9.0.2 version Z level problem

I had an issue like this in 10.0.1, that was fixed in 10.0.2.

Please have GTAC generate your path in the latest 10.0.2 and see if this has been corrected.

Mark Rief
Retired Siemens

Re: After NX 9.0.2 version Z level problem

Valued Contributor
Valued Contributor

Hey Mark ,

There havent been 10.0.2 yet in GTAC.

 

Also I am asking Why we need some different setting for this operation to work normally.

It was working true.  And also merge distance is using for tool path combination between cut area .  Now we can use  transfer using :none  transfer method : direct  . It's working .

Thanks everybody for helps .

Best Regards,

Alican

 

2015_06_12_08_28_03_Siemens_PLM_Download_Server_unigraphics_maintenance_release_nx10_win64_.jpg

Re: After NX 9.0.2 version Z level problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Mark is saying send your part to GTAC - the _GTAC folks_ DO have access to 10.0.2 (even though it hasn't been released to us normal users).  THEY can check you make sure your case is fixed (or if not, submit a PR so it can be fixed).

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: After NX 9.0.2 version Z level problem

Like Ken says - have a GTAC person generate the operation in 10.0.2.

 

Normally you should not have to change a setting to get the same path.

Mark Rief
Retired Siemens

Learn online





Solution Information