Cancel
Showing results for 
Search instead for 
Did you mean: 

Animation speed too fast

Pioneer
Pioneer

Hello All,

 

I have the animation speed for tool path verify set to 1.   It still goes too fast.   Is there a way to slow it down?

 

Thanks!

 

FMJ

3 REPLIES 3

Re: Animation speed too fast

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi FMJ,

 

Thank you for your request.

 

Would you mind sending your files to gtac, so that we can investigate this case?

 

Cheers,

Alexander

Lead Product Manager - Mold & Die

Re: Animation speed too fast

Siemens Phenom Siemens Phenom
Siemens Phenom

One thing you could additionaly try is using Simulate instead.


You can do that even without having a machine loaded.

Lead Product Manager - Mold & Die

Re: Animation speed too fast

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi FMJ,

 

with NX103/NX11 you can change the Minimum Simulation Time within the Simulation Settings in Manufacturing

 

2017-08-09 10_18_07-PowerPoint Slide Show - [NX11.0.X_CSE&Content_v4.pptx].jpg

 

Regarding the Minimum Simulation Time there are some background information:

 

The “Minimum Simulation Time” (MST) value is used to indicate how often a display update happens during simulation if speed slider is set to 1. The formula for the slider setting is like:
MST * 2^(n-1) - n is slider setting.
MST need to be a multiple of the cycle time.

 

The initial MST setting is within the kinematic model. To change this, open the kinematic model in Machine Tool Builder. Open Simulation Settings Dialog in Navigator (RMB)

2017-08-09 10_25_54-Simulation Settings.jpg

Learn online





Solution Information