Cancel
Showing results for 
Search instead for 
Did you mean: 

Another problem with hole_milling in NX10

Valued Contributor
Valued Contributor

Hello!

In NX8.5 I had following to tell the system, where the toolpath should start:

2015-07-23 15_01_27-Hole Milling.png

or

2015-07-23 15_01_56-Hole Milling.png

Regardless of the pilothole, the toolpath has been generated as specified

 

In NX10 I only have "Offset from Start Diameter" and the Start Diameter is allways the pilothole. If there is no pilothole I can say "Offset from Start Diameter" = 0 or 5 or 10 or 100, there is no change in the toolpath. 

 

2015-07-23 14_53_20-Hole Milling NX10.png

Is this behavior intendend or may it be that this will change again in next NX-version? Is it perhaps a bug?

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0
2 REPLIES

Re: Another problem with hole_milling in NX10

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

This was an intentional change and has been documented. It was done to align in with the new NX9 drilling which supports an In-Process Feature concept. The start diameter can now be inferred from a previous (drilling or hole milling) operation. It can be found within the feature geometry dialog.

I.e.In NX 8.5, if a Blank Distance of 5mm has been defined for a 20mm hole, it will turn into a 15mm Start Diameter in NX 9 and NX 10.

The "Offset from Start Diameter' is a parameter to sepcify how far from the Start Diameter to begin the cutting passes.

 

Thanks,

Oliver

 

 

Re: Another problem with hole_milling in NX10

Valued Contributor
Valued Contributor

Thanks Oliver.

Werner
Production: NX10.0.3, FBM | TcUA 10.1.2.2
Development: VB.NET, Tcl/Tk | Testing: NX12.0

Learn online





Solution Information